News
> Business & Finance
> Products
> Events & Shows
> Global news magazine
 
 
 
 
 
Danfoss Logo

Danfoss launches first mass produced VLT® Low Harmonic Drive

17 August 2009
Danfoss Industries Private Limited, a leader in mechanical and electronic components and solutions, today announced the launch of the first mass produced VLT® Low Harmonic Drive.

The latest addition to Danfoss’ prominent VLT series of Drives, the VLT® Low Harmonic Drive eliminates the harmonic disturbances on the supply grid by actively imposing currents into the grid so that the high quality sine wave of the grid current is restored.

“The issue of preventing harmonic disturbances is growing with the employment of more and more powerful frequency converters. Even after many years growth of the drives market, only one out of eight motors is operated by a frequency converter. We expect that the huge potential for energy savings will increase the need for drives – and in turn, increase the need for harmonic disturbance on the supply grid” said P. Ravichandran, Regional Vice President Asia Pacific, Danfoss Industries Pvt. Ltd.

Like other Danfoss VLT® drives, the Low Harmonic Drive is built on a highly modular technology platform which has been very successful in proving their functionality, quality and overall reliability in other parts of the broad VLT® drives program. The drive has the same modular build-up as Danfoss’ normal high power drives and share features like high energy efficiency, backchannel cooling and user-friendly operation. Due to the modular principle, most elements are produced in large scale, leading to cost effective production.

Since VLT® drives are all individually configured according to the customers specific needs – and only the VLT® Micro Drive produced to stock – the VLT® drives represent the value of a highly customised quality drive – for the price of a mass produced unit. Where the performance of other low harmonic technologies depends of stability and load or effect the controlled motor, the new Danfoss Low Harmonic drives continuously regulate the network and load conditions without affecting the connected motor. VLT® Low Harmonic Drives causes no increased winding stress or reduction of the bearing lifetime.

Available in the power range of 160 - 710 kW, the VLT® Low Harmonic Drive meets the toughest harmonic recommendations and gives the user full readout of the unit performance towards the grid including graphical overview of grid behaviour. The VLT® Low Harmonic Drive also meets the IEEE519 recommendation and is suited for generator powered installations like in back-up systems.

Passion and responsibility

The Danfoss Group has net sales of about DKK 16.4 billion (2.2 billion EUR) and employs more than 18,200 people worldwide.

Based on our core values, Danfoss’ vision is to be a global market leader within our core businesses: Refrigeration & Air Conditioning, Heating & Water and Motion Controls.

We aim to meet the expectations of our stakeholders by being a highly respected company, improving quality of life by mastering advanced technologies in customer applications, while focusing on environmental and social responsibility.