Refrigeration and Air Conditioning
> Products
> News
> Subscribe to the Danfoss APA Newsletter
> Technical Literature
> Software
> ICV
> The Industries We Serve
> Training and Education
> Heat Exchangers
> Contact
 
 
 
 
 
Danfoss Logo

Coolselector®: The Intelligent & Easy to Use Selection Tool

Coolselector is now updated to version 1.0.1.x which includes also compressors and condening units.

Coolselector now also installs on Windows Vista and Windows 7.

At the same time we have made instructions of how to install Coolselector on a network.

Please select your installation below:

New Installation of Coolselector

Please note that you must have Administrator Rights to the PC on which you want to install Coolselector.
Please click on the link below to install Coolselector.

Firefox & Chrome users: When asked, please download the "setup.exe". When done, please double-click the file in the Download Manager or in the download destination to continue the installation. Please repeat this with the file "Configurator.application"

I Have Coolselector Installed Already

Please first close your Coolselector!

Please note that you must have Administrator Rights to the PC on which you want to install Coolselector.

To install the new version of Coolselector you will first need to un-install the current version. Please click on the link below to renew Coolselector.

The installation of the new version will follow automatically. Please be aware of all the pop-up’s

Firefox & Chrome users:
When asked, please download the "Refresh.exe". When done, please double-click the file in the Download Manager or in the download destination to continue the installation.
Please do the same with the following files:
"setup.exe".
"Configurator.application"

Network Installation of Coolselector

Please fill in the form below to register a free CD with the installation files for installing Coolselector on a network.

Installations on networks should be done by qualified personnel only!

Disclaimer

All values calculated and components selected by this software must be verified by the user.
Danfoss can accept no responsibility for possible errors in the Coolselector program.

Danfoss reserves the right to alter its products without notice. This applies to products already on order, provided that such alterations can be made without subsequent changes in specifications already agreed upon.

©Danfoss A/S, Refrigeration and Air Conditioning Division 2010.