Marine
One of our main focus areas is the marine and combustion sector. As our sensor measures the emission of relevant gasses such as CO2, NO, NO2, SO2, humidity etc. in the exhaust from the combustion processes, our sensor can create value for the manufacturers and users of large combustion engines for propulsion or power generation.
The unique and patented construction of the Danfoss IXA sensor ensures accurate and reliable data input and long lifetime of the sensor even in the harshest environments.
When implementing technologies for reduction of NOx emission, the Danfoss IXA sensor can provide data on the effectiveness by measuring the humidity and NOx levels in the exhaust.
The Danfoss IXA sensor can give real time input from the combustion processes to the engine control systems and for monitoring purposes as described under the regulations of ie. MARPOL Annex Vl.