VLT® Taajuusmuuttajat
> VLT® Taajuusmuuttajat
> Uutiset
> Tuotteet
> Sovellukset
> Dokumentaatio
> Ladattavat ohjelmistot
> Kytkentäohjeita ja neuvoja
> Suunnittelijoille
> inMotion VLT Uutiskirje
> Tilaa VLT Uutiskirje
> Taajuusmuuttajien valintaohjelma
> Yhteystietomme
 
 
 
 
 
Danfoss Logo
Drive Configurator

Drive Configurator

The Danfoss Drive Configurator is a simple and easy to use tool to configure the exact Danfoss VLT frequency drive of your choice. The Drive Configurator generates the unique article number for the drive you have configured, preventing errors or mistakes when you order the drive. 
The other way around is possible too. Enter the article number you have and the Drive Configurator will tell you exactly for which drive this article number represents. With all options and special features that are included.   A big advantage of using the Drive Configurator is also that it tells you exactly which options and special features are avaible for the drive of your choice, also preventing you selecting options that can not be combined in one drive. Again this will prevent you of making mistakes when ordering the drive.  Last but not least the Drive Configurator will enable you to enter the article number of one of the older generation VLT drives and convert the old drive into a drive of the new VLT generation.

Use the link below to go to the Drive Configurator.