RESIDENTIAL SYSTEM DESIGN - AC OUTPUT
Ready for the grid
For residential installations you normally connect to the LV grid (low voltage distribution system). The house connection is usually the same as that of the PV system.
DLX inverter
The DLX inverter is single-phased. Therefore it is important to take grid regulations into consideration regarding the load limits on each phase.
TLX inverter
The TLX inverter is three-phased, and will feed a symmetrical output to the grid under all conditions - even if one or more DC inputs falls away.