Automatika i Procesi (AiP), the leading provider of Danfoss VLT Drives to the Croatian market, today announced the expansion of its products to include the Danfoss photovoltaic inverter line. “The team at AiP made a commitment to elevate Danfoss Drives to a top position in Croatia. We intend to bring this same level of success to Danfoss’ solar inverter lines,” said Milan Stanic, Manager of AiP.
AiP has secured terms with Danfoss Solar Inverters to become a Selected Sales Partner, distributing both the TLX & ULX inverter series.
· The TLX series ranges from 6.0, 8.0, 10.0, 12.5 & 15.0 kW
· The ULX series ranges from 1.8, 3.0, 3.6, 4.0 & 5.4 kW
The entry into the Croatian market is reflective of Danfoss Solar Inverters’ commitment to expanding its reach to new markets. “The high expertise and competency level of the AiP team with Danfoss products gives us a great deal of confidence that the Croatian market can prove to be very promising for us,” said Peter Westergaard, Regional Market Development Manager at Danfoss Solar Inverters.