TUS Opens New Supermarket with a Total Store Solution from Danfoss
20 February 2012
A brand new supermarket in Moravce in Slovenia is equipped with the latest Danfoss technology including the system controller AK-SC 255 which controls refrigeration, heating, cooling and lights. It also monitors and collects data which makes it a perfect system for energy savings.
The supermarket is part of TUS, one of the biggest supermarket chains in Slovenia. To the director of TUS, Mr. Brane Cokan, the total store solution is perfect for achieving energy savings: