The new version also offers the selection of electronic controls divided up into Pack Controls, Evaporator Controls, System Controls, Accessories and Frequency Converters
Coolselector® version 1.0.1.2 has also got improved calculations of several control valves such as thermostatic expansion valves, solenoid valves and other controls.
Do not miss out on all of these great new features - version 1.0.1.2 of Coolselector® is now available for download via the link below
Coolselector® is quite popular among many of our customers and is used worldwide, translated into 12 languages and has thereby become a great success for Danfoss. If you have not already got the software installed please visit our Coolselector® website today and download it. It is free for use both for individual users and for corporate distribution purposes.