New Improved Function Module for the Popular ICS Valve
08 February 2012
To meet the requests from our customers the one piece function module has been changed to make it possible to exchange some of the wearing parts instead of the whole module.
It has been a wish from some customers that it would be possible to exchange the Teflon seat because they experienced damage on the seat during start up due to dirt/welding particles in the system. We are therefore pleased that we have been able to make adaption to the product to accommodate this. With this change the whole size range from 25 to 150 can be serviced with the dedicated spare part kits.