Refrigerant compressors are used in many different applications. Some of these applications are special heat pump applications. One example is a dry cleaning machine, i.e. a professional application for drying of clothes.
The general purpose and function of a household washing machine should be widely known, so here is an ultra short technical summary: Water and detergents are mixed to create suds. The suds dissolve the dirt from the clothes. Suds and dirt are pumped into the sink. Fresh water is used to rinse the clothes to remove the remaining suds.
Dry cleaning machines use a chemical substance (instead of suds) to remove the dirt (Hence the name "dry cleaning": no water is used).

Fig. 4. Dry cleaning machine
The chemical substance Per (Tetrachlorehten) and increasingly a mixture of different carbon hydrates is used as solvent. The substances reach best cleaning results below normal room temperature. Therefore, refrigeration systems are used to cool the solvent. Water cooled condensers are often used in dry cleaning machines.
For obvious environmental reasons is not feasible to pump the solvent into the sink like the suds from the household washing machine. The dirt is removed from these substances by evaporating a part of the solvent in a separate tank. The solvent evaporates, the dirt stays behind. The refrigeration system is used to condensate and to recycle the solvent. Until this point, the refrigeration system is used only for cooling: one evaporator is cooling the solvent, another evaporator is used to recycle the solvent. The refrigerant usually condenses in a water cooled condenser.
Considerable amounts of solvent would remain in the clothes if they were taken out of the dry cleaning machine without additional processing. A so-called 'desodoration phase' is therefore initiated to remove the remaining solvent: warm air is blown through the clothes. The warm air evaporates the solvent and removes it from the clothes. The solvent is recycled using an air cooled heat exchanger with low surface temperatures, where the solvent is condensed. The warm air with solvent is guided to the air cooler. The air cooler is operated with low evaporating temperatures to recycle as much solvent as possible. The cold air is guided back into the dry cleaning machine via a second heat exchanger to heat it up again.
As an alternative to water cooled refrigerant condenser, an air cooled condenser is often used in the process. The heat from the condenser is used to heat the air for the desodoration phase. In this optimized setup the unit works in a heat pump cycle with double effect. Both sides of the refrigeration system are used: the cold side to recycle the solvent, the warm side to heat the air for the desodoration phase.
The different phases of a dry cleaning process result in different loads and demands for the compressor :
- Medium to high evaporating temperatures during the cleaning phase (solvent is cooled, condensing temperature depends on the set point of the water valve of the water cooled condenser),
- Low evaporating temperatures with medium to high condensing temperatures during the desodoration phase (heat pump mode with air cooled condenser).
It is necessary to have a reliable compressor operation under all these conditions.
Many compressors are equipped with internal motor protection systems.
Danfoss H-Series Performer® Scrolls are equipped with an innovative protection system which enhances the compressor protection at low evaporating temperatures.
This makes the Danfoss H-Series Performer® Scroll compressor a very good solution for this kind of application (e.g. a dry cleaning machine)
An internal motor protection should be placed directly onto the motor winding to react directly on the motor temperature. This gives a fast reaction and the optimum protection.

Fig. 5. Cut away Performer® Scroll Compressor HR-series
Figure 5 shows a cut away of the upper part of a Danfoss Performer® Scroll HR-Series.
In addition to the normal internal motor protection, the green plastic tube guides the oil coming from the cranks shaft and the bearings to the motor protector.
The rotating counter weight (coloured in magenta) creates a certain gas flow in the compressor. At high to medium evaporating temperatures, the gas density is high and the gas flow blows away the oil from the protector. This pre-empts an early and unnecessary cut out due to warm oil. In addition, the gas flow can transport heat from moving parts (e.g. bearings, moving scroll) in the compressor to the internal protector, which enables an indirect protection of these parts.
At low evaporating temperatures, the refrigerant gas density is low. The heat transport capacity of the gas flow is too low to ensure a sufficient indirect protection of moving parts.
However, the low density gas flow is no longer capable of blowing away the oil from the motor protector. Now the oil is used to "transport" the heat from the moving part to the motor protector to ensure the protection.
The end result is a high class compressor protection - even if the operating conditions change quickly like those of dry cleaning machines.
The examples mentioned above show that sound concepts, innovative ideas, and the right compressor choice for a given application lead to energy efficient and environmentally friendly solutions.