SGN+ is equipped with sensitive indicators that reflect a colour, depending on the moisture content in the refrigerant. They are suitable for HFC (including R410A) and HCFC.
- SGN+ is mounted in the liquid line to monitor the moisture content.
- SGRN+ is mounted in oil receiver or compressor to monitor the moisture content.
SGM+ is mainly used to indicate the condition of the refrigerant.
- SGM+ is mounted in the liquid line to monitor the refrigerant and can be used to see;
- If subcooling is insufficient (bubbles)
- If there is acid in the system (oil discoloured from light brown to black)

The code numbers remain almost the same. The "-" of the previous SG versions is replaced with an "F" for the new SG+ versions e.g. 014-0171 becomes 014F0171.

This, however, is not the case for SGH as they are now replaced by SGN+ as indicated in the table above. The introduction of the SG+ will be phased in over the coming months with a safety stock of the SG being gradually reduced as that of the SG+ is increased.
For further information on the SG+ stainless steel sight glasses please contact your local Danfoss sales office or Partner Wholesaler. Literature is also available for download from the local Danfoss website: www.danfoss.co.uk
SG+ SG