Pressure Drop
Generally speaking with the component selection the resultant pressure drop should always be considered. With the filter drier this is not necessary in every case, as it only has a marginal pressure drop in use with the respective pipelines. If you find a filter drier in an existing system, which, despite the usual condensing temperatures (e.g. 45°C and without a subcooler being installed), forms condensation or even ice on the pipe surface downstream from the filter drier, then the drier is most probably clogged up with dirt particles. With measurement connections before and after the drier, the service manometer then indicates a correspondingly high pressure drop when checked. In such cases there is no alternative but to replace the drier.
Drying Capacity
Looking at the respective datasheets we repeatedly see the term "drying capacity". This indicates the amount of refrigerant that can be "dried" by the filter drier for a specified refrigerant and specified temperature. This is based on the specific moisture content of the refrigerant before and after the drying process. A "DML" drier, for example, can therefore bring 8.5 kg of R134a refrigerant at 24°C from 1050 ppm to 75 ppm. "ppm" stands for "parts per million", and in a specific case indicates the number of water molecules (H2O) in the refrigerant per million refrigerant molecules. If the refrigerant charge volume of the system to be planned has not yet been specified, the suitable filter drier can also be dimensioned according to the liquid capacity. "Liquid capacity" is the cooling capacity in "kW" for installing the drier in the liquid line. The ppm values before and after drying can be confidently accepted by the system builder as practical; they are based only on the refrigerant and the refrigerant charge of the system.
Filter Drier with Replaceable Solid Core
If a standard drier is actually required, but the line connection sizes are already in the 7/8” or 22 mm and higher range, a housing filter drier can be used for swap-out drying blocks ("Danfoss DCR"). These housing filter driers are available for operation with one or more solid cores. The main advantage of this variant is the very easy exchange of the drying cores without any soldering or dismantling of the lines and the moderate service price, as the housing remains in the system and does not have to be bought again. The main application area for this housing drier is also the liquid line.
If, out of interest, you want to illustrate the enormous water absorption capacity and the high moisture volume that is bound together in the ambient air, then you can set-up the following easy example. You open a drier block core (e.g. "48 DM") and set the block on a scales. Now you note the weight and observe the colour of the drying core. A day later the colour of the drier will have darkened significantly and the weight will have increased considerably.
Conclusion
Filter driers are indispensable for a compression refrigeration system's smooth operation. If you shy away from the cost of configuring the filter drier via the drying capacity, you can choose the connection dimension and selection of the bigger model (bigger volume) for the corresponding pipe dimension. The pressure drop will then generally also be OK.