Refrigeration & Air Conditioning
> Refrigeration & Air Conditioning
> Products
> Products & Applications In Focus
> News
> Technical Literature
> Software
> Education and Training
> Market Segments We Serve
> Refrigerants & Energy Efficiency
> Exhibitions & Events
> About Us

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

Condensing Units

25 February 2011 | Author: Stephan Bachmann, Technical Support, Danfoss Germany
Useful practical tips for the everyday work of fitters is provided in the Fitters Notes series. The Fitters Notes series is based on the handbook of the same name produced by Danfoss, which discusses the basic principles of commercial refrigeration systems and the associated basic components.
Average user rating:
out of votes
> Click here to read the full article
Chapter 1. Condensing Units

The compressor is often described as the heart of a refrigeration system. However, for systems up to a certain capacity, refrigeration specialists often like to use a compressor integrated into a condensing unit. Air-cooled condensing units - which are the exclusive subject of this article - generally consist of a compressor (or sometimes two compressors), a condenser with one or two fans, an electrical terminal box, and optionally high-pressure and low-pressure switches and a receiver.

Preassembled Modules

There are also water-cooled condensing units, in which the air-cooled condenser with fans is replaced by a water-cooled condenser. Coaxial condensers are the preferred choice for relatively small condensing units, but they gradually give way to shell-and-tube condensers and plate heat exchangers as the capacity increases. The entire module is pre-configured with the tubing necessary for the refrigeration circuit, and the electrical connections are fed to a separate terminal box. This means that part of the refrigeration system is pre-assembled and does not have to be put together on site.

This yields distinct time and cost savings without reducing flexibility, since it is still possible to use a wide variety of evaporators and regulators.

Fans

The size of the condenser depends primarily on whether it is fitted with one or two fans. If there are two fans, which are normally arranged next to each other, the condensing unit is somewhat wider. If there is one fan, the base plate of the condensing unit is usually very compact. As a result, the complete unit is somewhat higher. Fan motors are available in single-phase and three-phase versions, with the vast majority of devices being fitted with 230-V, single-phase fan motors in actual practice.

There are two main reasons for this. As single-phase compressors are used in relatively small condensing units, a corresponding type of fan motor is also used. However, a 230-V fan motor is often used even with three-phase compressors operating from a 400-V supply voltage, since variable-speed control can be implemented less expensively for a single-phase motor. Pressure-led variable speed controls with phase-angle control are very widely used in refrigeration systems, and they can usually be retrofitted in standard condensing units as an option. However, it is necessary to pay attention to suitability for phase-angle control operation (or the insulation class of the fan motor), since fan motors become warmer with phase-angle control than without, which can lead to problems - especially during summer operation. The direction of air flow in a condensing unit is always suction through the condenser coil, and thus from the fan toward the compressor.

This ensures better air contact with the air-cooled condenser. If the fan does not rotate in the desired direction, this can be corrected with a 400-V fan motor by swapping two of the phases. With a single-phase fan motor with a capacitor, the direction of rotation can also be changed by swapping those two leads from the motor where also the two leads of the capacitor are connected. In case of doubt, consult the wiring diagram in the terminal box of the condensing unit.
Chapter 2. Receiver
A receiver is always present in the condensing unit when the system uses an expansion valve as a throttling device. If a capillary tube is used for injection in the evaporator - which is usually the case with very simple and small systems - a receiver is not included in the condensing unit. Receivers in condensing units for expansion valve operation are usually mounted upright. This is better for ensuring a reliable liquid reserve, especially if the outlet to the liquid line is taken from the top of the receiver via a dip tube and only a small residual volume of liquid is left in the receiver as a reserve. In condensing units with relatively large capacity, the receiver outlet can usually be shut off. This simplifies repairs to the refrigeration system that require opening the refrigeration circuit substantially. If the receiver outlet valve is closed, the refrigerant of the system can be pumped into the receiver. This makes it possible to carry out service work between the receiver outlet and closed suction side of the compressor without having to remove the refrigerant charge from the system.

Pressure Switches


Whether or not a condensing unit is fitted with high-pressure and low-pressure switches is primarily a question of price. However, at least a high-pressure switch must always be retrofitted. It is also not advisable to do without the low-pressure switch for cost reasons, because if it is not present when it is really needed - for example, in case of a loss of refrigerant - the result can easily be a defective compressor. From a business perspective, this is considerably more significant than the price of a low-pressure switch.

The high-pressure side of a dual pressure switch has divided refrigeration system builders into two camps for many years already. One camp always uses a pressure monitor (automatic reset after triggering) if this is allowed. The other camp always uses a high-pressure limiter (manual reset after triggering for restarting the system) to ensure that the high-pressure shutdown does not go unnoticed. For this reason, Danfoss condensing units with pressure switches have a special, pre-fitted version that allows the reset on the high-pressure side to be configured as individually desired. Either the automatic reset function or the manual reset function can be selected by shifting the position of a safety washer.
Chapter 3. Installation
Reliable performance of a refrigeration system with a condensing unit is particularly dependent on the installation. As a rule of thumb, the distance from the wall should be at least equal to the height of the condensing unit, with the direction of the emerging air stream facing away from the wall. This is necessary not only to ensure an adequate supply of cooling air, but also to allow regular cleaning ofthe coil with compressed air or nitrogen. Installing a condensing unit in a narrow air shaft creates the risk of a short-circuit in the air circulation. This means that the air that has just passed through the coil and been heated is sucked in and drawn through the coil yet again. This causes a strong increase in the condensing temperature and is thus not advisable. If the unit is installed outdoors, it is recommended to use an optional weatherproof housing.

A mistake that is often made in user-built constructions carried out after-wards by persons not specialised in refrigeration systems is severe restriction of the air flow past the unit. Here care must be taken to ensure that the condenser coil and the opposite side are left completely free. There is no objection to placing closed panels on the other sides or on the top.



Cooling Capacity

There is a special consideration with regard to specifying the cooling capacity of condensing units. The cooling capa-city is always specified at a particular ambient temperature (usually 32 °C). This may appear somewhat unusual, since a specific condensing temperature is normally taking as the basis. For example, the cooling capacity of a compressor is specified for a fixed condensing temperature of 50 °C or 54.4 °C, depending on the standard conditions. However, if the same approach were used with condensing units, the size of the condenser would not be taken into account. For this reason, the capacity of a condensing unit is measured at a specific ambient temperature (under laboratory conditions). This means that a condensing unit with a larger condenser has a lower condensing temperature, which means it has a higher cooling capacity even though the same compressor is fitted. This also reduces the difference in cooling capacity resulting from using different refrigerants, as compared to considering only the compressor.

In other words, if (for example) you compare the capacity of a condensing unit with R404A to the capacity of a condensing unit with R134a, you will see a smaller difference than if you compared the compressors fitted in the units. As R404A has a higher volumetric cooling capacity than R134a, a compressor operating with R404A has a higher capacity than the same model with R134a at the same evaporating temperature.

However, the condenser of a multi-refrigerant condensing unit will appear larger if R134a is used instead of R404A, so that the condensing temperature is lower than for operation with R404A. This improves the cooling capacity of the condensing unit with R134a. In short, in case of doubt it is a good idea to check the performance figures of the compressor when examining the performance specifications of condensing units.

Chapter 4. Multi-refrigerant Capability
This leads to the question of whether these differences in the refrigerating capacity of a condensing unit due to the refrigerant that is used can be utilised commercially. The answer is 'yes'. The first benefit is obvious: if the condensing unit is designed to be suitable for use with various refrigerants, such as R404A, R507, R407C and R134a, availability from the refrigeration wholesaler is better than if a different unit is used for each type of refrigerant. This benefit is especially important with relatively large condensing units, since they take up more space in the warehouse of the wholesaler (and space is expensive). The second benefit is increased customer flexibility. For example, if a new system is being built and the customer is not yet sure whether an expansion will be carried out in the coming years, it is advisable to install a condensing unit with multi-refrigerant capability and operate it with R134a. If the system is installed in a petrol-station shop, for example, and the shop is enlarged five years later, it is possible to extract more cooling capacity by simply changing the refrigerant to R404A without having to replace the condensing unit.

This is by no means detrimental to the customer, since R134a refrigerant has a very good energy rating and only rates second to R404A (or R507) in terms of general-purpose use.

Fully Equipped Condensing Units

Beside conventional condensing units with a basic configuration, fully equipped condensing units are presently very popular. With conventional units, features such as fan speed control, a weatherproof housing, compressor protection, an emergency stop switch, a dryer and a sight glass can only be retrofitted as options, they are already included in a fully equipped conden-sing unit outdoor module. 


These units are usually more compact than standard condensing units in terms of the required installation area. A standard unit provides time savings during installation, and the time savings with such a ready-to-install unit are of course even greater. The growing popularity of these complete units also has a positive effect on pricing. As a result, these units have become a genuine alternative, especially for demanding end customers. System builders espe-cially appreciate features such as integrated, pressure-controlled fan speed regulation and a built-in electrical cabinet with an emergency stop switch.

Working with you to improve your business

In everything we do our main principle is
to be customer driven to satisfy short and long term customer needs and expectations. Our aim is always to be perceived as being THE BEST CHOICE, PREFERRED PROVIDER and BUSINESS PARTNER.
Together we can improve your business.
So if you want the support of a company that works to improve the efficiency and profits of your business, call us today
We are here to make it happen