Refrigeration & Air Conditioning
> Refrigeration & Air Conditioning
> Products
> Products & Applications In Focus
> News
> Technical Literature
> Software
> Education and Training
> Market Segments We Serve
> Refrigerants & Energy Efficiency
> Exhibitions & Events
> About Us

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo
Food Retail - Danfoss Refrigeration & Air Conditioning

AKD LCP Simulation Tool

The tool demonstrates the ease of programming of the Danfoss Food Retail AKD 102 inverter by taking the user through the "wizard" set up guide.

The wizard has default settings for compressor, condenser fans, and single fan and pump applications.
The WinZip file below allows the user to download a commissioning simulation tool for the
AKD 102 local control panel, onto his computer.

Programming and commissioning is achieved by using the OK, and Up/ Down arrow keys only.
The 'info' button will also provide help if needed as this is a built in instruction manual.

Please click on the link below to download the AKD LCP Simulation Tool.

ADAP-KOOL® - "Solutions you can grow with"

Do you want to be kept up-to-date with Food Retail? Then sign up for our dedicated Food Retail newsletter.