What is the maximum/minimum pressure/temperature at which Danfoss switches can be set?
Answer: Danfoss manufactures various pressure switches which can have a setting range of anywhere between -1 to 400 bar and temperature switches from -60 to +300°C.
However, each switch will have its own regulation range as detailed within the product catalogue pages. It is always good practice to avoid choosing a product which will be switching near to the limits of its range.
What is the DIN numbering of terminals?
Answer: Terminal numbers are always ODD for inputs & EVEN for outputs, which explains why the changeover switch in almost all pressure & temperature switches has numbers 1, 2 & 4. The live feed goes in at 1. It comes out at 2 when the pressure or temperature is low (so take this to your pump or heater as a live feed) out of 4 when the temperature or pressure is high. (You can take terminal 4 to a ''satisfied'' tell-tale lamp or to an unloading valve or cooling fan, if you wish).
What is differential?
Answer: The differential is the difference between a switch cutting in and cutting out – it is like on a kettle after it has boiled and switched off, you can not switch it on again until the kettle has cooled down a little. Too small a differential will give rise to short running periods with a risk of hunting. Too high a differential will result in too large pressure or temperature oscillations.
I need a spare part for my product. Do you have that?
How can the differential in RT controls be adjusted?
Answer: To set a differential in RT unit, please use the diagram that can be found in customer instruction. The diagram shows which digit should be set at the differential setting disc to obtain required differential. The input to the diagram is differential range and neutral zone, which gives the setting position on the setting disc.
How can I characterize vapour charge in the sensor of the temperature switch?
What does it mean that an RT switch has an IP66 grade?
Answer: IP is a classification of enclosure grades. It contains 2 digits. The first digit indicates the degree of enclosure against foreign bodies and the second one indicates the degree of water tightness. IP66 means that a wire of 1 mm diameter and dust cannot enter, and that the enclosure will withstand water jets from all directions, 100 l/min.
How I can characterize adsorption charge in the sensor of the temperature switch?
Answer: The sensor is partially filled with carbon particles, and the rest of the element contains superheated gas, normally CO2. Reaction is always in the sensor and working point will vary with the ambient temperature.
After installing the switch and making the setting based on scale values, the real system pressure value and scale value seem not to correspond. What is the reason?
Where can I find approvals and certificates for Danfoss products? E.g. do you have a PED certificate for KP7W?
What is the time constant in relation to temperature switches?
Do Danfoss products comply with RoHS directive (Restriction of Hazardous Substances)?
Answer: Yes, all declarations of conformity, including RoHS and WEEE, can be found in our internet product catalogue. Look up the product of your interest and find the relevant document either under the Literature link or the Approvals & Certificates link.
I am looking for the on/off switch with the highest possible IP protection, what options do I have?
How does the manual reset work in relation to on/off switches?
What is differential setting (pressure or temperature)?
What does SPDT stands for?
What is the most common contact system type used in Danfoss switches?
What would be the best pressure switch choice for applications requiring high repeatability, accuracy and adjustable differential?
When is it recommended to use a gold-plated contact system?
What is the key difference between KPS and CAS switches?
I have bought a sensor pocket for KPS temperature switch with the code no. 060L326266 but am missing accessories.
I'm looking for a Danfoss code number and I have not found it in any catalogues?
Answer: Som code numbers are not available for all markets, or it may have been replaced by another number.
To resolve the issue, please contact your nearest Danfoss office: http://www.danfoss.com/Contact/Worldwide/
I am looking for a Danfoss product, type USC6000, but cannot find it in your catalogues?
How can I improve the heat transfer if I use a sensor pocket with a temperature switch?
Could I send you a Danfoss part for repair?
I am looking for a pump, type APP?
Can you explain the function and shape of the RT 102 thermostat's sensor?
Answer: The sensor of the RT 102 thermostat consists of 2 parts: A 2 m capillary tube, diameter 3 mm and 1.1 m capillary tube, diameter 4 mm, which is a "real" sensor with active carbon inside.
The RT 102 with such sensor can be used for temperature measurement in a duct. It is important that the entire active carbon sensor (4 mm diameter) is in the duct.
Where I can find technical information regarding on/off switches?
Is it possible to change the set point in a pre-set KP temperature switch, e.g. from 35°C to 29°C?
Why is there no information regarding scale correction in the technical brochure for a KP temperature switch?
Answer: Because the ambient temperature influence depends on 2 factors: 1) size of a sensor and length of the capillary tube, and 2) value of the ambient temperature.
KP switches usually have smaller sensors than KPS switches, and they are installed in less severe conditions than KPS, so ambient temperature influence is very small and could be omitted.
I am looking for Danfoss MASSFLO and MAGFLO flow meters?
I am looking for a Danfoss butterfly valve?
Do I need an external power supply for RT switches?
Can you deliver your products wordwide?
Answer: Yes, we have own distribution centres across the world, working together with more than 100 distributors and agents. You can see your nearest distributor or Danfoss office here: http://www.danfoss.com/Contact/Sales_and_Services/
Do you have a complete catalogue showing all your products?
Answer: Our internet product catalogue is the most extensive information source: http://www.danfoss.com/Products/Categories/
Besides these products, Danfoss also produces customer-specific products and solutions that are not visible in the catalogue. Please contact your nearest Danfoss office to discuss your needs and how we can meet them.
Can you deliver products exclusively made for us?
Answer: Yes, we have the possibility to develop products that are unique for one customer subject to individual agreements. The products may differ in appearance, technical features or packaging. Please contact us to discuss your requirements.
Which distribution channels does Danfoss use?
Can I review your stock online?
Where can I find technical drawings of Danfoss products?
Answer: Dimension and function drawings of our products are often part of the products' technical leaflets. In our internet product catalogue (http://www.danfoss.com/Products/Categories/), find the product of your interest, then follow the Literature link to see avaliable items.
Where do I direct commercial or technical questions?
Do you have local stock?
Where can we find your data sheets?
Answer: All relevant literature, including technical brochures, are available on our Web site: http://www.danfoss.com/BusinessAreas/IndustrialAutomation/Documentation/Industrial+Automation+Literature.htm
Do you have local websites in my language?
Is it possible to place orders online?
Can you give me some key figures on danfoss?
Answer: If you are looking for number of employees, sales companies, turnover etc., you will find updated information here:
http://www.danfoss.com/AboutUs/FactsAndFigures/
Does Danfoss operate globally?
Is Danfoss a German company?
I am looking for a hydraulic oil pump?
Is it possible to order an MBC with short cable and special plug (different then DIN plug)?
Is there any way to tell if charge is lost in a temperature switch?
I am looking for a KP temperature switch for a small load: 10mA at 110V dc. Is it preferable to use gold contacts for this application?
Answer: Although amperage is quite low, standard silver contacts can be used because the voltage is high enough. If in doubt, the gold-plated contacts can be used. In cases where the load is too high, the golden layer will be burnt away and silver contacts will remain.
A diagram showing when gold plated contacts shall be used is available in the technical brochure, downloadable from our internet catalogue.
Why is our delivery delayed, when I saw that the delivery date is confirmed for 2 weeks in e-commerce?
Where can I find some technical information about your products?
Is it possible to recognize if a RT has "double" bellows installed, from just looking at it from outside?
What do I need to know to select the right product?
Do Danfoss temperature switches come with sensor pocket included?
Can I get quality control plans/process flowcharts/material specifications/FMEA for Danfoss products?
How do I maximize response time of a temperature switch?
Answer: First, the sensor should be immersed in the media with biggest possible surface. If this is not possible and a sensor pocket is needed, remember that the additional thermal inertia of the pocket will play a significant role. You can use heat conductive paste to reduce it.
What do I do if I need very quick reaction to changing temperature?
Answer: In case of any mechanical switch with charge sensor, the reaction time will always be a considerable factor. The solution could be using a temperature sensor, which has much smaller themal inertia.
What is the response time of Danfoss temperature switches?
Answer: There is no exact data on the time constant for temperature switches in particular - it largely depends on sensor charge, way of mounting (contact to media), temperature changing speed, ambient temperature and other factors.
Can you send me literature, brochures or catalogues on your products?
I placed an order through e-commerce. Could you please check the delivery dates and inform me the earliest possible delivery?
Which temperature switch should I use to control the area temperature in an engine room?
Can I download product approvals & certificate from the Danfoss websites?
Answer: Yes, in our internet product catalogue, all product approvals & certificates are listed. If you are unable to local a specific document, please e-mail or call us.
Can I order just the capillary tube for an AVTA?
Is it possible to buy just the contacts for the RT switches?
Which media can Danfoss products be used with?
Answer: The answer depends on the materials in contact with medium for the particular product. This information can be found in the technical brochure / data sheet for the product.
We have products designed specifically to handle particular media, including drinking water, oil, air, petrol, steam and more. If in doubt, please contact your nearest Danfoss office.
Which switches should I use for seawater - or other media with particles or depositions?
Answer: In case of seawater you should generally use diaphragm versions of switches:
- KPS 43, 45 & 47
- CAS 143, 145 & 147
- MBC 5100 with diaphragms
Seawater may contain contamination and certainly salt, both of which will likely accumulate inside the application. Not least inside the switch,, because the water inside is almost still (no flow). If salt crystallizes on the bellows surface it can easily affect its proper function.
In case of diaphragms, very smooth and flexible, this problem is less visible. This will cause the depositions to be removed from its surface, and until the whole system is filled and blocked with depositions, it will work.
Depositions are especially dangerous when you have a small bellows - like in MBCs.
If you need to use bellows version of switches then try to choose comparatively big bellows - surfaces on which depositions are stored are comparatively far away and it would take a longer time before they affect bellows function. RT is a switch of this kind.
Where do I find production date on pressure or temperature switches?
For the Pg plugs sold with MBC, which are the recommended cable diameter sizes?