Danfoss valves keep Czech train toilets flushing despite the cold
28 June 2010
In autumn 2004, České Dráhy (Czech Railways) signed a contract with fellow Czech company, Pars Nova, for the supply of 130 railcars. Operating on regional routes, the railcars have a preassembled vacuum toilet module, with a built-in pressurised water system – and Danfoss solenoid valves were chosen to control the water system. Designed specifically for use in closed circuits with low differential pressure, the EV250B empties the railcars’ water tanks and makes sure the toilets will keep flushing for years to come, even in freezing conditions.