Industrial Automation
> Products
> Industries
> Documentation
> News
> News Archive
> Exhibitions
> Service Request and FAQs

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo
Pressure transmitter

Danfoss helps clean up drinking water in Mexico

23 April 2009
Access to safe drinking water was recognised as a basic human need at the 5th World Water Forum recently. In Mexico, however, reliable access to clean drinking water is a problem for many of the country’s 111 million inhabitants. Major investments in water projects are now being made to guarantee that at least 95 percent of the population has access to clean drinking water by 2012. And Danfoss is part of the drive.

Keeping the pressure on

In northern Mexico, fresh natural water resources are both polluted and scarce. In the central and far south-eastern regions, water is inaccessible and poor quality. In fact, access to clean water has become such a problem in Mexico that the government considers it a national security issue. Providing a reliable supply of clean water has been high on the government’s agenda since early 2008. New water purification projects are underway throughout the country – and the local Danfoss office is busy keeping up with demand for components.

In Mexico, reverse osmosis systems are commonly used to purify water. In reverse osmosis, pressure forces a solvent from an area of high solute concentration through a membrane to an area of low solute concentration. Pressure transmitters, pressure switches and solenoid valves help maintain the right pressure in the system, and Danfoss components are doing the job.
Pressure Transmitter in reverse osmosis system
A Monterrey-based company is using the Danfoss MBS 3000 pressure transmitters and the KPI switches in their reverse osmosis system. Featuring excellent vibration stability, robust construction and a pressure range from 0 to 600 bar, the MBS 3000 is ideal for water treatment. Compact and versatile, it performs well even in the harsh conditions in Mexico’s tropical areas and deserts. The KPI 35 and KPI 36 pressure switches are used to control and monitor liquid and gaseous media, and can cope with pressure ranges from 0.2 to 28 bar, and a high contact load.

Contact your nearest Danfoss office for more information on our extensive product portfolio.


By Diogo Francisco Guirau Hernandes, Sales Manager
Industrial Automation Products

Industrial Automation product catalogue

Dive into our product catalogue and find details about our industrial products:

Read more about our industrial products and applications:
Feedback Form