VLT® Drives
> Home
> Products
> VLT FlexConcept
> ECplus Concept
> Drive Configurator
> Manuals, Approvals and Drawings
> Brochures & Factsheets
> Software Downloads
> Fieldbus Communication
> Connecting & Programming your VLT drive
> Industries We Serve
> Case Stories
> Service & Support
> News & Press
> About ...
> How to ...
> Contact Form
> VLT Newsletter Subscription

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

Reduced power consumption and improved productivity at Indian sugar mill

18 June 2009
The installation of a 750 kW VLT® AutomationDrive on the main mill has reduced power consumption significantly and improved productivity for JHV Sugars Limited at Padrauna, Uttar Pradesh, India.

The performance of the drive system has measured up to the end user’s expectations. Mr. M. K. Biswas, Group Head (JHV Sugars), has expressed his satisfaction at the outcome and will now consider replacing the remaining three turbine driven mills with motor and VLT® drive.
Replacing steam turbine
JHV Sugars Limited, a reputed manufacturer of cane sugar with business interests in distilleries, decided to use the Danfoss VLT® drive for a mill crusher in their sugar plant. The decision was part of a modernisation programme aimed at replacing the steam driven turbine with AC motor and drive. The order also included a 225 kW drive for the ID Fan and a 90kW drive for the juice pump.

Vast experience
Key reasons for choosing Danfoss were its vast experience with supplying drives for various applications in sugar plants and the positive feedback from other customers in the industry regarding the performance of VLT® AutomationDrive and Danfoss’ ability to provide quality application knowhow and service at short notice. The Main Mill drive was installed and successfully commissioned in February 2008 during the crushing season, along with the other drives. Its performance to date has been entirely satisfactory.

Excellent overload handling
Due to the varying load requirements and the high overloads experienced during cane crushing, the mill drive is usually specified for an overload duty corresponding to IEC Class IV or Class V.

The requirements of these duty classes are as detailed below:

Class IV:
100% Continuous, 125% for 2 hours and 200% for 10 seconds, where the base load (torque) is 100%.Gurgaon , India

Class V :
100% Continuous, 150 % for 2 Hours and 200 % for 60 seconds.
Considering Class IV duty with overloads already factored in, the continuous rating of the drive motor was specified as:


Continuous capacity:     750 kW.
Operating Voltage:       415 V ±10 % 
                                  50 Hz ± 5 %.
Synchronous Speed:     1000 rpm
Rated Current:             1303 A.

Since the motor rating was specified with overload, the drive continuous rating was matched with that of the motor. The choice fell on the VLT® AutomationDrive, model FC302P800T5 with a constant torque rating of 1460 A and an overload capacity of 150% for 1 minute.

Fully tested
The F Frame drive was fully tested with the locally manufactured incomer ACB panel prior to dispatch to site. The newcomer’s apprehensions regarding the drive performance were laid to rest once the load trials were successfully conducted in February 2008.

Positives
Many positives accrued from the installation of the drive system and motor:

• 20 % lower start torque
Due to the acceleration ramp function in the drive, it was now possible to set an appropriate ramp up time (90 seconds) and ease the starting requirements on the mill with the existing diesel generator set. The power consumption requirements during mill start were significantly lowered, the reduction being ≈ 20 %.

• Current within motor ratings
Operation in VVC+ Control mode resulted in good speed holding characteristics and ability to handle the overloads encountered during normal running of the mill. An examination of the key parameter plots shows that the maximum drive current (monitored using the MCT-10 drive software’s trending feature) during crushing is 1008 A, which is well within the motor and drive FLC ratings.

• Simplified control requirements
Mill speed is now controlled by adjusting the motor frequency instead of steam flow control with flow control valves as was the case with the turbine. The control requirements are thus considerably simplified.

• Maintenance costs lowered
With the introduction of a standard squirrel-cage induction motor, the running costs on account of maintenance have been significantly lowered.
Danfoss VLT Drives Social Media

We keep you informed the way you want it

Do you want us to keep you informed on Twitter, or do you prefer to use Facebook.

You can also subscribe to our VLT Drives inMotion e-newsletter or watch the videos on our YouTube channel. 

• New product features and options
• Updates of technical literature
• Software upgrades
• Fairs and exhibitions
• Seminars and workshops
• Interesting applications and developments in your field

We make this information available through different channels. It is up to you to choose the one that fits you best.
Feedback Form