New VLT® Decentral Drive is presented at Drinktec in Munich, 14 - 19 September
27 August 2009
The succesor to the renowned decentral VLT® drives is presented at the Drinktec fair in New Munich Trade Fair Center, 14 - 19 September.
The VLT® Decentral Drive FCD 302 is the new generation of the VLT® Decentral FCD 300, based on the VLT® AutomationDrive FC 302 platform. It combines the key features of both products in a completely re-designed enclosure, made for best fit on direct machine mounting. Simplicity and robustness have been taken into consideration during the design of the new VLT® Decentral Drive FCD 302, resulting in a real user-friendly product, offering high performance and the highest protection degree.