The third element of the Login block is your preferred language. The availability of different languages is a function of the way in which the system is set up in your country, but normally English will be offered as an alternative to the local language.
If you access the Login Screen without having access to the system, you may use the Request Access link (see below) to do just that.
Resolution of issues relating to access for an existing account can be initiated by clicking the I can not access my account link.