VLT® Drives
> Home
> Products
> VLT FlexConcept
> ECplus Concept
> Drive Configurator
> Manuals, Approvals and Drawings
> Brochures & Factsheets
> Software Downloads
> Fieldbus Communication
> Connecting & Programming your VLT drive
> Industries We Serve
> Case Stories
> Service & Support
> News & Press
> About ...
> How to ...
> Contact Form
> VLT Newsletter Subscription

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

New Luxury in Copenhagen - The Climate-friendly Hotel

A completely carbon neutral solution is not yet possible, say the owners of Crowne Plaza Copenhagen Towers.

But the new luxury hotel in Copenhagen’s Ørestad district comes close to achieving it by deploying the best environmental and energy technology on the market. Including Danfoss VLT HVAC Drive frequency converters.

Hospital cuts energy costs with VLT® Drives

Aarhus University Hospital in Denmark expects to slash its energy consumption used for cooling by 800,000 kWh per year after installing new, VLT® HVAC Drive controlled chillers and heat pumps.

The drives were installed in a complete overhaul of the hospital’s cooling and heating system. The new system is one of the first to combine heating and cooling in a single system and will reduce the hospital’s CO2 emissions by 750 tons a year.

Energy savings up to 78% and optimum conditions for elephants, jaguars and penguins

VLT® drives from Danfoss and a ‘demand matched’ ventilation strategy has resulted in energy savings of up to 78 % being recorded for Chester Zoo in England; 55% of the savings are directly attributable to the drives, which in addition contribute to an unforeseen animal welfare improvement.

VLT® HVAC Drives control pneumatic mail system for sensitives samples

The Innsbruck University Clinic extended and modernized an existing system to make it the most modern pneumatic mail system in Europe. The required pressure is provided by more than 100 frequency controlled bellows - controlled by Danfoss VLT® HVAC Drives saving money on energy, maintenance and wear and tear.

VLT® HVAC Drives improve internal hospital environment – reducing energy consumption by 50%

Danfoss VLT® HVAC Drives enable the hospitals’ Building Management System to respond to changes in outside air temperature, duct pressure and temperature providing versatility, reliability and energy savings to the Brighton & Sussex University Hospitals.

Belfast International Airport lowers its carbon emissions by 500 tonnes per year

Annual energy savings will top 1,000,000 kWhrs in Belfast International Airport after refurbishment of several of the terminal’s air handling units with electronic motor controls.

Clean performance for clean blood

ASEM-NPBI is the world leader in products for blood collection and processing. The company is building a new factory in Brazil and the installation of Danfoss VLT® variable frequency converters in the HVAC system is helping to ensure that the factory’s Clean Room meets the strict contamination control standards.

Danfoss keeps things tuned up at the Kennedy Center

Danfoss VLT® Series drives were applied in the new variable volume air handling solutions, to replace the old constant volume motor starters for America’s living memorial to President Kennedy at The Kennedy Center in Washington, D.C.

Danfoss offered a narrow vertical configuration for drive installations. Danfoss was also able to adhere to a strict delivery time requirement, which became another key factor in winning the order.

Proven VLT® quality in Kuala Lumpur Mall project

Danfoss Drives provide drives for office towers 2 and 3 of The Garden Mid Valley project in Kuala Lumpur. The shopping mall project valued at USD 180,000 with 140 x VLT® 6000 IP54 drives were delivered with support of the owner and consultant.

VLT® AutomationDrive saves EUR 15.000 every year

The Dutch company Royal Ahrend N.V. Ahrend was able to realize these considerable savings and a significant reduction of noise with only a relatively small investment. Because only one VLT® AutomationDrive was driving seven motors over a long distance.

VLT® control keeps SS Great Britain shipshape and Bristol fashion

A major aspect of that work is to stabilise the wrought iron hull and protect it from the ravages of further corrosion. The most innovative part of that work consists of constructing a sealed glass plate around the waterline of the ship to form a giant airtight chamber surrounding the ship’s lower hull.

Beneath the water surface - separated by a glass plate - moisture is removed from using a specially designed air-handling unit operated 24 hours per day, 7 days per week by VLT® 6000

VLT® drives for 12 leading brands of data storage media

Moser Baer is OEM supplier to all the 12 leading storage media brands in the world. Danfoss presented AHF Solution to the customer and had marathon discussions to convince them to go ahead with a trial on 4Nos.

Moser Baer observed the performance of VLTs & AHFs. Convinced with the much superior harmonic performance of VLTs & AHFs and significant average energy saving of over 30% on each AHU, Moser Baer placed another order on Danfoss for supply of 40 VLTs, AHFs and Flow Sensors.

VLT® drives pay back in 9 months on boiler fans

Following the installation of a VLT® drive on an 11 kW boiler forced draft fan, Dairy Crest has achieved energy savings of over 47,000 kWh per annum, reduced associated carbon emissions by 5.52 tonnes per year and achieved a payback on the investment in only nine months.

“In addition to saving us money, the drive has made my life a little easier through reduced maintenance requirements on the boiler." - Craig Pepworth, Dairy Crest.

VLT® HVAC drives will keep Hyderabad International Airport cool

Danfoss India is going to furnish the prestigious Hyderabad International Airport Limited with VLT® HVAC drives for air handling applications. 148 pcs. VLT® drives rating from 2.2 to 37 kW will be installed in the passenger terminal block.

The secondary chilled water system and pressure booster water supply system for this project are also being supplied with Danfoss drives.

Heating, Ventilation and Air Conditioning

Danfoss has unequalled experience in advanced drive technologies for HVAC applications. This experience has been used to optimise features in the VLT® drives and make it the perfect match for pumps, fans and water chillers (compressors) in buildings fitted with sophisticated HVAC solutions.


Products: