VLT® Drives
> Home
> Products
> VLT FlexConcept
> ECplus Concept
> Drive Configurator
> Manuals, Approvals and Drawings
> Brochures & Factsheets
> Software Downloads
> Fieldbus Communication
> Connecting & Programming your VLT drive
> Industries We Serve
> Case Stories
> Service & Support
> News & Press
> About ...
> How to ...
> Contact Form
> VLT Newsletter Subscription

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

Drive Configurator

The Danfoss Drive Configurator is an advanced but easy-to-use tool to configure the Danfoss VLT® frequency converter that exactly matches your requirements.

The Drive Configurator generates the unique article number for the drive you need, preventing errors during order entry.

"Reverse engineering" is also supported: Enter an article number and the Drive Configurator will display the exact configuration for the drive in question, including all options and special features. A further advantage of using the Drive Configurator is that it tells you exactly which options and features are avaible and so prevents you selecting conflicting or nonsensical combinations. 

If you need to replace an obsolete product, just enter the article number of the older VLT® and the Drive Configurator will provide details of the appropriate newer generation replacement.

Last but by no means least, the Drive Configurator provides quick access to the available spare parts and accessories for both current and obsolete products.

Click on the link below to explore the Drive Configurator.
Danfoss VLT HVAC frequency drives

VLT® drives make a difference to the Chinese air traffic

A total of 830 VLT frequency drives was used to ensure reliable electrical system performance in high profile Chinese airport projects.

Beijing Capital International Airport, Terminal 3.
The construction was completed in 2007 and Danfoss Drives delivered a total of 330 VLT®6000, drives, rated from 1.1 to 315kW.

Shanghai Pudong International Airport, phase 2 was also completed in 2007. Here Drives delivered 150 VLT®6000 and Advanced Harmonic Filters rated from 1.1 to 315kW.

Shanghai Hongqiao International Airport was completed in 2009. For this task Drives delivered 350 VLT® HVAC Drives and Advanced Harmonic Filters drives, rated from 1.1 to 250kW.

These three orders are high-profile, showpiece projects. The consulting engineers responsible for the building activities and the end-users (the airports), were convinced of the excellent Drives HVAC system performance and Danfoss’ low harmonic performance.
Feedback Form