VLT® Drives
> Home
> Products
> VLT FlexConcept
> ECplus Concept
> Drive Configurator
> Manuals, Approvals and Drawings
> Brochures & Factsheets
> Software Downloads
> Fieldbus Communication
> Connecting & Programming your VLT drive
> Industries We Serve
> Case Stories
> Service & Support
> News & Press
> About ...
> How to ...
> Contact Form
> VLT Newsletter Subscription

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

200+ Danfoss VLT® drives boost reliability in a harsh working environment

The high efficiency and innovative backchannel cooling system of the VLT® High Power Drives made them the first choice for a 600,000 tons/year calcium carbide plant in Inter-Mongolia, China.

Despite extremely severe site conditions, the VLT frequency drives have proven to offer the best possible reliability.

VLT® 690V high-power frequency converters optimise large-scale fermentation process in China

Novozymes is the world’s largest producer of industrial enzymes. VLT® AutomationDrive series frequency converters are used to control mixers, blowers, compressors etc..

VLT® drives optimise oil production in Texas

At an oil well in Texas VLT® drives maintain an optimum pressure balance between oil wells and surrounding reservoirs. More oil flows into the wells, thereby raising overall production.

Using a VLT® drive to vary the speed of certain parts of the stroke can minimize this stress, making the components last longer. This can be accomplished while still maintaining the same number of strokes per minute, which keeps production up.

High tech suture material for the medical industry in Korea and Japan

According to Managing Director Richard Slack “We selected the new Danfoss VLT® AutomationDrive for a number of reasons. In addition to the accurate vector control, there are a number of features on the AutomationDrive that simplified their adoption and gave us confidence to meet the demands. Not least of these is the ability to connect the drives on an Ethernet network, which enables us to interrogate the machine set-up remotely."

Clean cut – safe cut

The PLASCUT 591 from cutter specialist MAGURIT uses the VLT® AutomationDrive with its ”Safe Stop” feature to ensure the speedy and safe opening of blood plasma packages.

Drugs and vaccines based on blood and blood plasma are crucial in the treatment of many illnesses or injuries, such as bleeding disorders, immune system deficiencies or extensive skin injuries. Therefore, all handling of blood related products needs to take place under controlled, clean and safe conditions.

Danfoss VLT® 6000 HVAC works 24 / 7 to maintain air conditioned cleanroom environment in a life savings drugs plant

When India’s leading drug maker Cipla decided to build a world class drug manufacturing plant at Goa, it chose the Danfoss VLT® 6000 HVAC drives to control around 350 AHUs and 20 Pumps to maintain inside conditions and differential pressure in the manufacturing areas.

About us

With our Vision and Core Values as foundation, Danfoss lives up to the expectations being a responsible world citizen.
This is deeply rooted in our history and culture and it shall be reflected in the way we carry out our daily business.

Danfoss' relationship with all stakeholders shall be characterised by trust. We are, of course, aware that trust must be earned through our actions and corporate reputation.