Product Categories
> Refrigeration and A/C
> Heating
> VLT® Drives
> High-Pressure Pumps
> Industrial Automation
 
 
 
 
 

Solenoid valves

113 Item(s)

FAQ

  • Why does the valve not close?
  • Can the Danfoss solenoid valves operate by themselves or do I need to buy other things?
  • What IP ratings do the valves have?
  • What happened to the code numbers for the WRc approved valves?
  • Why does the solenoid valve not open?
  • Why does the solenoid valve sound wrong (humming)?
  • I have a coil here - which valve can I use?
  • Can you supply valve coils for hazardous areas?
  • What is a kv-value?
  • What is the difference between direct- and servo-operated solenoid valves?
  • Which media are your solenoid valves suited for?
  • I need a spare part for my product. Do you have that?
  • If my system has back pressure, should I take any precautions?
  • Where can I find approvals and certificates for Danfoss products? E.g. do you have a PED certificate for KP7W?
  • Do Danfoss products comply with RoHS directive (Restriction of Hazardous Substances)?
  • I'm looking for a Danfoss code number and I have not found it in any catalogues?
  • I need a solenoid valve for a machine for use in North America, do you have some?
  • Could I send you a Danfoss part for repair?
  • Can I test if my solenoid valve is working properly without mounting it in the system?
  • Do you offer steam valves complete with coil?
  • Which valve should I use for pressure relief function in an open system with high pressure?
  • Are the code numbers of the EV220B solenoid valves the same as the previous EVSI valves?
  • Which valve should I choose for an aggressive fluid?
  • Can Danfoss supply a solenoid valve with the coil mounted?
  • Can I use the EV220B with chlorine?
  • Which solenoid valve should I choose, if am not sure about the differential pressure of the application?
  • I am unsure about the pressure conditions in the installation, and I need a solenoid valve, size 1” - which should I choose?
  • Does Danfoss offer a timer for solenoid valves?
  • Can I buy Concordia valves?
  • Does Danfoss offer products with ATEX certificate (EEx)?
  • Do you have sparepart kits for the EV valves?
  • Can you supply the Danfoss valve with the type designation WKB?
  • Do you have a Danfoss solenoid valve with code number 018F7251?
  • What is the difference between the EV220A and EV220B solenoid valves?
  • Is it possible to order EV225B solenoid steam valves without coil?
  • I would like to energize my solenoid valve for a short time with a controlled sequence - what could I do?
  • Is it possible to order only the coil for Danfoss solenoid steam valves?
  • My solenoid valve or coil is making a unpleasant noise, what could I do to fix it?
  • Do you have solenoid valves for air compressors?
  • Can I use the EV220B solenoid valves for steam applications?
  • I would like to order a solenoid valve with the stamped no. 446U5252 and can not find it in your system?
  • How do I see if the coil of the valve is energized?
  • Can you deliver your products worldwide?
  • Do you have a complete catalogue showing all your products?
  • Can you deliver products exclusively made for us?
  • Which distribution channels does Danfoss use?
  • Can I review your stock online?
  • Where can I find technical drawings of Danfoss products?
  • Could I use any Danfoss coil for the B-series valves ?
  • What is differential pressure?
  • What is water hammer?
  • I need an EV220B 1/2" for an open water system. Which one should I choose?
  • What does servo-operated mean? Has it to do with servo control?
  • Can I mount an EV220B valve upside down?
  • I have mounted an EV220B valve in the warm water circuit of a heating system. The valve does not open. Is it defect?
  • Is it possible to use the Danfoss solenoid valves on natural gas installations?
  • I have ordered an EV220B valve NO, but if I blow through the valve, it is closed. Have I got a NC valve?
  • How can I see if my solenoid valve is NC or NO?
  • Can I order only the upper part of a valve housing as a spare part?
  • Where do I direct commercial or technical questions?
  • What are the difference between direct-, servo- and assisted lift operated valves?
  • Why does Danfoss not offer EV250B valves in bigger sizes than 1"?
  • Why is an EV220B solenoid valve more expensive than an EV220A valve?
  • Do you have local stock?
  • Can I buy the sensor of a RT temperature switch as a spare part?
  • Where can we find your data sheets?
  • Do you have local websites in my language?
  • Is it possible to place orders online?
  • Is AM230C a Danfoss valve?
  • Does Danfoss operate globally?
  • Is Danfoss a German company?
  • Can I order a solenoid valve with a 380V AC coil assembled?
  • Can we offer a valve according to EN161?
  • Can I test the function of a solenoid valve by moving up and down the energized coil?
  • How can I connect a solenoid valve with a pressure/temperature switch?
  • What type of seal material is appropriate for glycol ?
  • Can I use the EPDM seal material for air?
  • My solenoid valve is not working. What could be wrong?
  • The solenoid valve EV250B is leaking. What should I do?
  • Is it possible to order a normally open (NO) version of the solenoid valve EV220B 65-100 Cl?
  • How can I replace 032U7328?
  • I assemble air suspension system for cars, does Danfoss have any solenoid valve for this kind of application?
  • I have a Danfoss solenoid valve in NO (normally open) version. Is it possible to change this valve to a NC (normally closed) version?
  • What is the difference between the EV220B and EV250B valves?
  • I am looking for a gas valve for Argon application for a closed system, which valve could I use?
  • Can you send me a UL certificate for EV220A and an A-series coil?
  • Does the Kv value correspond to the value of the flow?
  • Where can I find some technical information about your products?
  • Can I buy a pilot filter separately for flange solenoid valves EV220B 65-100 CI?
  • Is it possible to install an EV220B (15-50 series) on vertical pipes?
  • Does Danfoss offer a solenoid valve KIWA approval, necessary to approve a water pump module?
  • Which solenoid valve should I choose for Glycol as a medium?
  • I have an EV220B 25B that does not close properly - should I unscrew the equalizing orifice to close it?
  • What do I need to know to select the right product?
  • Are the solenoid valve Kv values valid for compressed air?
  • Can I get quality control plans/process flowcharts/material specifications/FMEA for Danfoss products?
  • Can you send me literature, brochures or catalogues on your products?
  • I placed an order through e-commerce. Could you please check the delivery dates and inform me the earliest possible delivery?
  • Which solenoid valve should I choose for showers?
  • Does Danfoss provide a solution for pressure control of screw compressors?
  • I work with steam and the Danfoss solenoid valve EV225B does not have enough flow. Can you recommend another option?
  • Which coil type fits the EV220B valve?
  • Which coil should I choose to get a Normally Open (NO) valve?
  • Do you have a solenoid valve for air, 24 V dc and 1/4" thread on both sides?
  • Can I get Danfoss solenoid valves suitable for seawater?
  • Can I download product approvals & certificate from the Danfoss websites?
  • Are EV250B valves suitable for vacuum?
  • What does "solenoid" mean?
  • Can I an EV220B valve for vacuum?
  • In a open water system, I have an EV210 valve which does not open - what can be wrong?
  • I think my valve coil has short circuited, caused by water. Can I order an O-ring to place under the coil?
  • Are your valves certified for use with water?
  • Which media can Danfoss products be used with?