News
> Business & Finance
> Products
> Global news magazine
 
 
 
 
 
Danfoss Logo

China Refrigeration Exhibition 2012 - A Success for Danfoss

02 May 2012
The 23rd China Refrigeration Exhibition was held in Beijing, China in April. Danfoss industrial refrigeration attended this great event with many of Danfoss' leading solutions and newly introduced products.

The Danfoss booth was built on the concept of “dragons ride clouds to fly to the sky”, a visual depiction of both the wide open space and also of the free flying ability of the dragon. to symbolise how Danfoss' combination of technologies and solutions in energy saving can enjoy an ever increasing developing space.
Danfoss industrial refrigeration used the China Refrigeration Exhibition to display its new Flexline™ flexible platform including the ICF Control Solution, the ICV industrial control valve and the SVL series line components. The Flexline™ concept is based on the modular system that allows application-specific solutions to be tailored from just one body. The maximum pressure which the Flexline™ products can withstand is 52 bar. Furthermore, it is suitable for all flammable and non-flammable refrigerants (including CO2). It is a flexible application solution for the future!

The new liquid level sensor for Industrial Refrigeration, namely the AKS 4100U was also on display at the Danfoss booth, and won the “Innovation Award” for its advanced TDR (Time Domain Reflectometry) guided radar technology. This competitive technology helps to give a more accurate liquid level reading and also resistance of oil interference. Furthermore, it is easy to both install and maintain. 

Also on display at China Refrigeration 2012 was the Danfoss STC series stop valves, which adopt the teflon valve plate and O-ring sealing to realize higher safety levels. The extraordinary back seating function of the STC enables the replacement of the spindle seal, which can effectively reduce downtime.

Overall, the China Refrigeration Exhibition 2012 gave Danfoss plenty of opportunity to show off our many innovative solutions for industrial refrigeration. We will be back next year in Shanghai with more energy saving solutions for your refrigeration applications.

Innovative products and service

Danfoss Refrigeration is taking the lead in the use of new technologies to offer simpler, better and more cost effective
solutions. Solutions that improve refrigeration processes and lower maintenance and energy costs.We have already introduced advanced networking solutions for monitoring and controlling processes, remotely if needed. And we do everything we can to make it easy for you to procure and deploy the solutions you
need.