Corporate Citizenship
> Corporate Citizenship
> Policies and obligations
> Global initiatives
> Human and Labour rights
> Anti Corruption
> Society relations
> Supplier relations
> Climate and CO2 emissions
> Environment
> The REACH regulation
> Danfoss Negative List
> Corporate Citizenship reports

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

Environment

Danfoss is a global industrial group with strong competencies within energy efficient solutions. Since its foundation in 1933, the group has based its work on the fundamental respect of efficient use of Nature’s resources.

The philosophy behind the first Danfoss products was to make optimal use of energy while minimising waste, in the best way possible.

According to Danfoss’ simple philosophy, money saved today through reduced energy consumption is money that can be invested in green technology in the long run. And the solutions to energy savings already exist.
With existing and well-proven technology, it is possible to immediately cut the energy consumption in a range of industries and societal sectors.

Environmental management

Danfoss is a global company, and takes co-responsibility for sustainable development in the areas and countries in which the group is operating. The group’s policies concerning working environment, environment and social responsibility ensure high managerial focus on the compliance with national and international guidelines and declarations.

Danfoss has production facilities in around 60 locations worldwide and, therefore, impacts the surrounding environment in the form of noise, waste, the emission of flue gases and waste water. It is Danfoss’ clear objective that nowhere in the world must the production result in an unacceptable impact on the environment. Furthermore, the environmental impact is required to decrease over time and lead to a reduction of the group’s overall impact on the surrounding environment.  

Factories with more than 20 employees are required to be certified according to ISO 14001, and all Danish factories are also required to be certified according to OHSAS 18001. However, one Danish factory still needs to become certified.
In 2009, the group had 56 factories that are set to be ISO 14001-certified, of which 51 have been certified, while the remaining are working on certification.

Since the 1990s, Danfoss has had sharp focus on avoiding using substances and materials which could have a harmful effect on humans or the environment. The list of the unwanted substances is called the Negative List and it also applies to suppliers.  

Corporate Citizenship

Danfoss’ overall goal within Corporate Citizenship is "keeping our own house in order".
This applies to employees, so that they have an attractive workplace and a healthy working environment. It applies to the environment, where Danfoss products contribute to energy savings, and where the environmental impact of their production is constantly being reduced.
And it applies, in a broad sense, to social and ethical responsibility.
Efforts are continually being intensified, because when employee satisfaction is high, consumption of resources is as low as possible, and the company’s ethics and reputation are good, the result is a positive effect on the accounting bottom line.
Feedback Form