Corporate Citizenship
> Corporate Citizenship
> Policies and obligations
> Global initiatives
> Human and Labour rights
> Anti Corruption
> Society relations
> Supplier relations
> Climate and CO2 emissions
> Environment
> The REACH regulation
> Danfoss Negative List
> Corporate Citizenship reports

Follow us:

Danfoss on Facebook Danfoss on Twitter Danfoss on LinkedIn Danfoss on YouTube
 
 
 
 
 
Danfoss Logo

Environmentally-friendly washing system at the Bellows Factory in Nordborg

At Danfoss’ Bellows Factory in Nordborg, the reconstruction of the washing system has resulted in major environmental gains.
The factory has halved the consumption of chlorate oil used as a lubricant in draw and extruding processes (equalling an annual reduction of 3,000 litres) by centrifuging the workpieces, gathering the excess amount of oil and reusing it. The factory has phased out the use of kerosene for cleaning chlorated oil from certain workpieces. The kerosene has been replaced by alkaline detergents which have made it feasible to lower the temperature in the rinsing and soap containers by 20 degrees. This has made it possible to change the heat source from electricity to district heating generated from natural gas. Thanks to this shift, the factory has obtained annual savings of around 300,000 kWh.  

In addition, the soap water container has been fitted with a sloping bottom and a foot valve which permits the separation of the deposited oil – thanks to which a 50% annual reduction of the chlorated waste oil (200 tonnes) has been obtained. Furthermore, the factory has obtained considerable water savings by recirculating rinsing water through a charcoal filter and an ioniser. The consumption of rinsing water has been reduced from 13,000 to 3,000m³ per year. Demineralised water is used for the next rinsing in order to avoid stains of scale on the workpieces. This water is also recirculated and as a result the consumption has been reduced by almost 90 per cent to 240m³.

Corporate Citizenship

Danfoss’ overall goal within Corporate Citizenship is "keeping our own house in order".
This applies to employees, so that they have an attractive workplace and a healthy working environment. It applies to the environment, where Danfoss products contribute to energy savings, and where the environmental impact of their production is constantly being reduced.
And it applies, in a broad sense, to social and ethical responsibility.
Efforts are continually being intensified, because when employee satisfaction is high, consumption of resources is as low as possible, and the company’s ethics and reputation are good, the result is a positive effect on the accounting bottom line.
Feedback Form